About file saving
- 4-1How can I add a specific string before or after the file name?
 - 4-2How can I change the file name?
 - 4-3How can I specify the file save location?
 - 4-4When I make changes to dimensions and specifications in RAPiD Design(inCAD Components), will the original file be overwritten with the edited file?
 - 4-5How can I save the file even though the part is a nonstandard state?
 - 4-6Can I use "Pack & Go"?
 - 4-7What is a file with the name "BaseModel~"?
 - 4-8How can I use the same component in a different size?
 
About technical information
About mates and constraints
- 4-10When mates and constraint components are edited in RAPiD Design(inCAD Components), are the mates and constraints transferred?
 - 4-11Can I save components imported with mates and constraints separately with RAPiD Design(inCAD Components)?
 
About assembly
- 4-12Can specifications and dimensions be changed in the assembly file?
 - 4-13How do I save a part or assembly file?
 
About configuration
About performance (operating speed)
About properties
About the operating environment
Precautions for use
- 4-18Why is there a discrepency between the model and part number?
 - 4-19Why is the model recognized as a "Not standard parts"?
 - 4-20Are the specific materials set for parts and assemblies?
 - 4-21What happens if I delete features in SOLIDWORKS?
 - 4-22Can I change dimensions using the Hole Wizard?
 - 4-23What are the differences between "Apply to CAD model" and "Save with part number"?
 - 4-24Why is there no fine screw thread shown in RAPiD Design(inCAD Components)?
 - 4-25Why are there specific dimensions required for some alterations?
 - 4-26What does the "Older Version File" warning means?
 - 4-27Which software version shall I use?
 - 4-28What does the message "Information relating to the model" means?
 - 4-29Is it possible to double log in?
 - 4-30Is it possible to run multiple instances of SolidWorks simultaneously?
 - 4-31What is the problem if nothing is showing up on the startup screen of RAPiD Design(inCAD Components)?